Part Number: DAC80508
Hi team,
I would like to know whether there's any operation I need to do before I sending read / write SPI commands to operate DAC80508?
I tried to read DAC80508 register DEVICE ID register by issuing 0x82, 0x00, 0x00, and trigger another data cycle after 1ms for retrieving read result, as figure below.
However, I got nothing while I issuing second data cycle, what might go wrong?
The operating conditions is as below:
VDD = 5.0 , VIO = 3.0V, Temperator = 25°C