Part Number: ADS42JB69EVM
Other Parts Discussed in Thread: ADS42JB69
Hello,
I have a ADS42JB69EVM connected to KCU105 through the FMC connector.
I'm having a problem recieving sync codes when the FPGA drives the sync low.
Afetr power up, I load the .cfg file throu the TI EVM GUI and configure the Xilinx JESD204 IP.
I can see the sync driven low but the code is not received.
The interesting part is that if I change (in tab ADS42JBXX) "SYNC Request" from "Normal Operation" to
"Generate SYNC Req", I can see the right codes on all the lanes, so I don't believe it's a connection problem.
I can also send it successfully through "Link Layer Test Mode".
I will appreciate any guidance to resolve it.
Thank you,
Kate