This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5562: Input power in dBm of differential pin of device.

Part Number: ADS5562

Hi,

I'm going to develop by using ADS5562 AD converter.

In this time, I want to know the following items.;

   1) how much is Input power in dBm of differential input port? I designed the method inputted by single-ended signal as evalution board circuit using two transformer.

    

   2) how much is the clock reference signal(pin-10, CLKP) by CMOS input condition?

    

  • Jarden,

    I do not understand your first question. No matter what your input power is in dBm, just make sure the voltage on each analog input pin is VCM +/- 0.9V. This should be 0.6V to 2.4V.

    For the second question, this should be at least 0.4V and no greater than 3.9V.

    Regards,

    Jim

  • Hi Jim,

    My question_1) means that I want to know what is input power of ADS5562.
    ; 1) how much is Input power in dBm of differential input port? I designed the method inputted by single-ended signal as evalution board circuit using two transformer.

    Regards,

    Jaden
  • Jaden,

    Are you saying your board has the same analog front end circuit as the ADS5562EVM and you want to know how much signal amplitude you can use on the single-ended input and stay within specification of the ADC?

    Regards,

    Jim