Part Number: ADS8689
Other Parts Discussed in Thread: OP07, ADS8695
There is a 10% error in the data obtained from the output of ADS 8689. Is there any cause?
The initials are set to unipolar 0V ~ 10V.
After sending the command [32'b1101_0000_0001_0100_0000_0000_0000_1001], read the value of ADC.
※ English may be strange. I'm sorry