Part Number: ADS1298
Hello,
I am implementing a circuit for sensing 8 biological signals (EMG) in differential mode using one ADS1298. My intention is to have a unipolar power supply of 1.8V for DVDD and 3.3V for AVDD (which will be supplied by an ODROID), to use an internal voltage reference and no electrode for RLD. The connection to the ODROID is through SPI with the 4 regular communication channels.
I am wondering if someone can check my schematic (attached) and help me in the case there are errors? I am especially concerned with the ADS pins 35, 52, 60, 62. I will not exclude errors in other pins...
If there is any extra information that I forgot to give, please ask.
Thank's in advance,
Best,
Sofia Rafael
P.S. In the schematics, the conditioning circuit at the left is repeated for each of the differential inputs