Part Number: ADS1293
Hi:
We used ADS1293 as the ECG sampling chip in a dynamic electrocardiogram (DCG) device.In the process of use, the following problems are found:
1. Separation problem:In the ecg sampling data record, it is found that the bias voltage of ecg signal is different in different human body or different time.It is not at the zero point (the position is random, it feels that this chip is not directly biased);But the horizontal line in the ADS1293EVM User's Guide image is at 0.Want to consult is how to achieve, we can carry on the circuit adjustment.
2. 50Hz interference problem