Part Number: ADC128D818SW-LINUX
Other Parts Discussed in Thread: ADC128D818
Tool/software: Linux
Dear experts,
I have a strange issue with ADC128D818 & standard Linux driver.
The device detects and seems to work well. The problem is that it takes ~ 1 sec to get a correct reading.
When I change voltage on a input pin and read continously, changes cannot be detected more frequently than once in a second.
Read itself (from the driver's sysfs file) is quick and does not hang. But updates do not occur at the rate that I need.
Any ideas, please? Can the driver be tweaked somehow to read faster?
The machine is iMX6 Solo (arm7), Ubuntu 14.04 LTS, kernel 4.1.0
Thanks,
- Pavel A.