Part Number: DAC8411
Other Parts Discussed in Thread: DAC8801,
I was testing a DAC8801 using the DAC8801 Eval board. The SPI signals are coming from ports on an STM32F407 and are all about 3.3V signals. The DAC8801 worked very well, but we decided we needed a voltage source and wanted to eliminate the external amplifier. So we had a DAC8411 overnighted to us and connected it to the same setup using a 5.0V supply for +5VA. The DAC8411 supply is 3.1V. It didn’t work. When I checked the SPI signals SYNC (CS) looked good, but SCLK and DIN were badly loaded. The SPI signals are configured with an active pull up. I added 1K pullup resistor on the CS, the SCLK and the DIN signal, pulled up to the +3.1V supply. This improved the DIN signal, but the SCLK amplitude is still only 0.5V. When the STM32F407 is connected to the DAC8801 all of the SPI signal amplitudes are 3.1V. Do you have any idea why the DAC8801 is loading my SPI signals? We have a very tight schedule and need to get this working in the next couple days.
Thanks,
Bob