Part Number: DAC38RF83
Hi!
I'm designing with DAC38RF83. In the datasheet in the electrical characteristics (p.17) it's stated that the input current on CMOS digital inputs can be in the range from -40 to 40 uA.
At the same time on fig.70 (p. 72) it's seen that these inputs have 10kOhm pull-ups/downs and, consequently, should have the input current no less then 1.8V / 10kOhm = 180uA.
So, what is the truth?
Regards, Victor.