Part Number: DAC43608
Dear Specialists,
My customer is considering DAC43608 and has questions.
I would be grateful if you could advise.
---
We believe that when ESD is applied to a circuit that is protected against ESD by external ESD protection circuit , it may be abnormal condition such as latch-up.
At that time,
(1)Does CLR return to normal operation?
Products from the competitor device currently in use will operate normally again with only the CLR.
(2)Or does the device need to be power on reset?
It seems to depend on the device's situation, what do you think.
I’d like to make the circuit as simple as possible and the cost as low as possible.
If possible,I do not want to add external circuits.
---
I appreciate your great help in advance.
Best regards,
Shinichi