Part Number: ADS114S06B
Hi, I'm using this ADC to convert two kind of signals, 0-60mVcc / 0-10Vcc, please see attached schematic.
I need to measure 0-60mV on AIN0 channel and 0-10Vcc on AIN2 channel.
Problem found: When I apply a signal higher then 2 or 3 Vcc on my input signal, reading AIN2 channel, I have wrong values.
When I open R7, I have the right values.
But I'm using 10K(R7) exactly to protect over current on AIN0 channel.
Can you help with this issue?
Thanks!