This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: Connecting 6 ADS1299s to a MSP432P401R Launchpad with SPI

Part Number: ADS1299


I am working on a project where I need to measure the voltages of 48 batteries continuously for about 3-4 minutes for a project. I plan on using 6 ADS1299s to measure the 48 batteries with differential inputs since the batteries are connected 8 parallel columns with 6 series batteries on each column. I am looking to read the batteries at a rate of at least 2 samples per second. I have some experience in working with an MSP432 and coding it so I set the registers and pins in the correct manner, but I was wondering if anyone can first confirm my idea will and if so, give me a rough idea of what I need accomplish coding-wise. Any help would be much appreciated as this project is a little out of my depth.