This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300: Can I duty cycle the 1MHz clock input to conserve power?

Part Number: AFE4300

Hi, I am thinking of using an external clock source with a lower power mode enable pin (stops sending a clock). I will be running single-shot mode on the AFE4300 and I was wondering if I could turn off the external clock source whenever the AFE4300 is in power down mode.