Other Parts Discussed in Thread: TMS320C5535, , THS4031
I want to interface ADS7883EVM with TMs320C5535 dsp.
kindly suggest how to start.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to interface ADS7883EVM with TMs320C5535 dsp.
kindly suggest how to start.
The ADS7883is a serial interface for communications. The CS SDO and SCLK pins need to be driven by the processor, this can be done using connector P2. Table 4 of the Users Guide also provides P2 connections
Power supplies can be provided through J2 connector, and the input signal can be conditioned with the onboard THS4031 using J1 or blue wired is past it on the R25. If the RC filter is not desires then R11 can be used to blue wire the input signal to directly connect to the ADC
The Users Guide has a schematic and helpful information.
Regards
Cynthia
Atul,
If you are looking for software support for DSP, I suggest you create a new post on the DSP forum.
As for the hardware, I have provided information as how to start off. If you experience any issues, or have specific questions then comment back here and I will try to address them.
Regards
Cynthia