Part Number: DAC38J84EVM
Other Parts Discussed in Thread: DAC38J84
hi,
We are having the DAC EVM DAC38J84 and KC705 evaluation board.
we want to implement the reference design slac690c which implements the JESD204B interface
To work with this reference design we need the TSW14J10 FMC-USB Interposer Card to communicate
with the HSDC pro software.
at present we have only the DAC38J84 EVM and KC705 EVM( XILINX FPGA).
we need to remove the functionality of TWS14J10 from the reference design.
to do the above process we need answers for the following quaries
1 . What are signals going from HSDC pro software to FPGA trough SPI interface?
and what is the JESD204B configuration it is sending to FPGA?
and how do we configure JESD204b ip without the TSW14J10 board in the reference design?
2. we are programming the DACEVM register using the DAC GUI. but it is
mentioned in the TSW14J10 user guide that using HSDC pro is able
to control the register of DAC .
what is the configuration that is written into DAC EVM using the HSDC pro ?
3. without using TSW14J10 can we use HSDC pro software to collect ADC data or
send pattern to DAC?
Thanks and Regards
Suraj Gaonkar