Part Number: ADS1230
I have a question regarding to ADS1230. Question is following:
What logic level appears on DRDY/DOUT pin, when PDWN pin is set to L?
I would expect Hi-z, but diagram o datasheet page 19 shows Hi!
Thanks
Ludek Pavlus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1230
I have a question regarding to ADS1230. Question is following:
What logic level appears on DRDY/DOUT pin, when PDWN pin is set to L?
I would expect Hi-z, but diagram o datasheet page 19 shows Hi!
Thanks
Ludek Pavlus
Hi Ludek,
Welcome to the TI E2E Forums!
The ADS1230 does not have a /CS pin to tri-state the nDRDY/DOUT as you might expect with most SPI devices. During power-down the nDRDY/DOUT will remain driven.
However, I'm not 100% sure if the nDRDY/DOUT will be forced high when you put the device into power-down mode. It may be that nDRDY/DOUT will retain its previous state into power-down mode.
Does that answer your question?