Part Number: ADS54J66
Hello,
My customer has questions about ADS54J66 as follows.
Q1
At the step 2 in the Table 72 (Recommended Power-Up Sequence) of the datasheet, “4001h 00h” and “4002h 00h” can be removed, but other sequences are all valid?
Q2
When broadcast is disabled (write address 4005h with 01h), how user can specify one of four A, B, C and D, although CH bit can set only two digits, 0 or 1?
Q3
When power down by Register 26h bit7=1 and bit6=1, JESD Bank Page register contents are held or cleared/back to default?
Best regards,
K.Hirano