I use tow ads8668 for sampling 16 channels of AC analog input with a ±10.24-V input range by daisy chaining。I select the internal reference, the
REFSEL pin be tied low or connected to AGND. So,the voltage of the pin of refio should be 4.096v,but infact it is 3.77v and 4.4v。and the sampling voltage uplimt lower than the reference volatage(2.5x4.096).I dont know the cause,please help me 。