Other Parts Discussed in Thread: ADS1298
So lets say I have a device based on the ADS1299 that works as a 8 channel EEG.
I have another independent device based on ADS1298 that works as a 12 lead ECG.
Both of these devices may be independent or may be not so these can lead to 2 scenarios.
Scenario 1
Both devices working on independent power supplies powered by batteries and are in no way linked to each other.
Scenario 2
Both devices working on common 12VDC supply but their grounds may not be common.
___________________
My question is since both devices are providing bias electrodes respectively. How do you prevent a conflict of these bias. Will the EEG bias affect the ECG and vice versa. How do commercial products prevent this? do they have a provision where devices or products can share.
The EEG bias would generally be attached to the earlobe or somewhere thereabouts whereas the ECG bias is attached to the right leg? These are quite distant locations. So is it a cause for concern fo the biases causing jumbled up signals would this cause a degradation of 50Hz signals not being correctly removed due to 2 simultaneous biases being injected into the human body?