Other Parts Discussed in Thread: ADS1258
One more thing, I understand the datasheet states that the ADS1258MRTCTEP, outputs data in the SPI interface that reports the gain error of the device (.5% max) and the reference reading error (1% ==> 3%) when it is sampling input signals. I'm assuming this means that software/firmware can read those errors in the datastream, which would allow those measurement errors in particular to be factored/canceled out of the measurement reading? For instance if a differential analog signal of 100uV is fed into the ADC, it is possible for software/firmware to look at the gain errors and reference reading errors during that measurement, cancel out those error factors and calculate the exact actual value of 100uV seen directly at the input?