Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299EEGFE-PDK: Interfacing MMB0 with Python

Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299

Greetings, Antony here.

Is it possible to interface the ADS1299EEGFE-PDK with the MMB0 EVM board using Python and obtain EEG signals?

Our current setup consists of the above, directly attached to the PC via the USB B port on the MMB0 board.

We are working on obtaining P300 signals using the above setup. 

  • Hi Antony,

    Thanks for your post and welcome to the forum!

    I am not an expert with Python, so I cannot be sure that it will work. 

    Writing the code is ultimately up to the customer so I cannot offer much help. The sample code for the EVM in the BIOFAQ link in my signature may be of use. 

    If you have specific questions for the ADS1299, please create a new thread and we'll be happy to help.