Part Number: ADS1261EVM
Hallo,
my Deta-Sigma ADC EvaluaTion shows no Registermaps in Device Region. Status says Hardeware Connected Ready and on Console i see Device ID and FW iD.
EvaluaTion was installed first and then the Device Package and the Driever then manually.
My System is Windows 10 and it is running wthout Admin rights. The installation did the Admin for me.
Am I right, that the Register Maps should be shown automatically if the device is recognized?
Could be there a Problem with rights if it is not?