Part Number: ADS62P45
Hello,
My customer has a question about ADS62P45.
[Q]
Please tell me the default value of the all registers. (address = 0x00 to 0x2F)
Best Regards,
Hiroshi Katsunaga
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS62P45
Hello,
My customer has a question about ADS62P45.
[Q]
Please tell me the default value of the all registers. (address = 0x00 to 0x2F)
Best Regards,
Hiroshi Katsunaga
Hiroshi,
After a reset is issued, either hardware or software, everywhere it mentions "DEFAULT" in the register description section of the data sheet (see below), will be the default setting. The example below shows a default setting of 00 for bits D7 and D6. If a register bit is unused, it will always be "0". These values will all be in an unknown state until a reset is issued.
Regards,
Jim
D7–D6 <CLKOUT STRENGTH> Output clock buffer drive strength control
01 WEAKER than default drive
00 DEFAULT drive strength
11 STRONGER than default drive strength (recommended for load capacitances > 5 pF)
10 MAXIMUM drive strength (recommended for load capacitances > 5 pF
Hi Jim,
Thank you for your response.
In the description of the D/S, there are cases where the register bit is used but the default value is not described.
For example, "SERIAL READOUT" (0x00, D0), "LVDS CURRENT" (0x11, D[3:2]) are not described the default value.
There are many more of these.
Therefore I confirmed to you the default value for each address.
It is OK with each address or each bit not listed in D/S.
Could you please check and tell me ?
Best Regards,
Hiroshi Katsunaga
Hiroshi,
After resetting the device, you can read out all of the registers via SPI. This is will tell you default values since the default register values are set after reset.
Thanks
Yusuf
Hi Yusef,
Thank you for your response.
OK, I understood your comment.
Thank you for your cooperation.
Best Regards,
Hiroshi Katsunaga