Part Number: ADC12DJ3200
Hi,
We are operating ADC12DJ3200 in interleaved mode. A single board has eight of such ADCs. While the data capture of all the ADCs is OK. The data capture of one of the ADCs is as shown in the attachment. The Fs/2 component in the frequency domain plot is also very high. The ADC input frequency is set to 2.1GHz and Fin 100MHz. We suspect this to be an issue with the ADC interleaving. Please advice.