Other Parts Discussed in Thread: ADS52J90
Hello,
SETUP:
hardware used: TSW1400, ADS52J90
software used: HSDC Pro GUI v5.0
HMC-DAQ GUI V2.8
Matlab code used: C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\HSDCPro Automation DLL\Manual and Examples\Automation DLL Matlab Example\64Bit Matlab
PROBLEM:
when I use the provided matlab code, ADC device can be selected and the HMC-DAQ GUI can be launched by HSDC Pro GUI, however, the HMC-DAQ GUI setup cannot be automatically setted, for example, item 3, choose data Format cannot be automatically chosen. I need to manually set them. But if I manually set them up, the configuraton settings in the later code such as 'Passing ADC Output Data Rate', 'Set ADC INput Target Frequency' will not be valid. Is there a way, that the Matlab code can automatically setup the HMC-DAQ GUI as I want?
Best regards,
Yu