Dear all:
1, I plan to use CC3220 to communicate with ADS7142 through I2C to support continuous sampling up to 40-ksps.How do I set it?
2,If the ADS7142 cannot support continuous sampling, are there any other devices recommended?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all:
1, I plan to use CC3220 to communicate with ADS7142 through I2C to support continuous sampling up to 40-ksps.How do I set it?
2,If the ADS7142 cannot support continuous sampling, are there any other devices recommended?
Hi,
Our ADS7142 expert is out of the office for a couple of days. I did however have a chance to talk to her. To do some sort of continuous sampling you would use the manual mode to configure and get the data. 40-kSPS should be an achievable rate.
Joseph Wu
Hi Joseph:
Thanks for your reply.
But use the manual mode to configure continuous sampling,Need to provide continuous SCL signal, this unless hardware add SCL clock chip?
I've tried using software that doesn't seem to work? so let's see if we can generate SCL signals from hardware.
In addition, if the hardware generates SCL signals, and the data we read is also through I2C, it will conflict with the SCL again.
Could this problem be solved?
But use the manual mode to configure continuous sampling,Need to provide continuous SCL signal, this unless hardware add SCL clock chip?
I've tried using software that doesn't seem to work? so let's see if we can generate SCL signals from hardware.
In addition, if the hardware generates SCL signals, and the data we read is also through I2C, it will conflict with the SCL again.
Could this problem be solved?
Hello,
creating the SCL signal through hardware will pose issues, mostly sync issues.
Would you explain why your software did not work to communicate with the device?
If you would like to explore other devices, would you please let me know what are the requirements? From this post, I assume a 2 channel device, I2C with minimum throughput rate of 40kSPS?
Regards
Cynthia
Hi Cynthia:
thanks for your reply.
Using the software method, we also need to trigger the CLK, which we don't want to do in this way.
other devices,Only those that can support continuous sampling above 140kSPS, 2-channel, simple operation, or above this specification are acceptable to us.
thank you!
Timsen,
Every device will need a SCL signal to output data, even if it is continuous or not. Data transfer cannot happen without a SCL signal.
I would suggest reaching out to the CC3220 team and solve your software issue, or confirm that the CC3220 can/cannot provide a SCL signal and how to do so.
Regards
Cynthia