A number of the bits in the registers are marked as reserved in the device datasheet.
What value do I write to these bits when updating the other fields in the register ?
Do I need to read-modify-write on all these registers, or can I just write 0 to the reserved bits ?