This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF85: Datasheet Register Reset Values

Part Number: DAC38RF85

The Register Maps section of the datasheet appears to contain 3 different sets of reset values for each register.

  1. There is a reset value in the section header for each register.
  2. There is a "value after reset" for each bit in the register in the Figure that is at the start of each section for each register.
  3. There is a Reset value for each of the fields in the register in the Table Field Description for each register

The values in these are not consistent for many of the registers.

What is the difference between each of these "reset" values ?

  • User,

    These values should all be the same. If you are seeing inconsistencies, there is a chance it is an error in the data sheet in Table 42. If you are concerned about a certain reset value, I would suggest doing a hard reset on the device and read back the register value.

    Regards,

    Jim