Hi Team,
My customer is curious about what's the biggest size of the screen TSC2013-Q1 can cover, if it can cover above 11-inch?
what's the parameter of the device related to the size of the screen?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is curious about what's the biggest size of the screen TSC2013-Q1 can cover, if it can cover above 11-inch?
what's the parameter of the device related to the size of the screen?
Thanks.
Hi Lucas,
Great question! The TSC2013-Q1 has a 12-bit resolution, which means the device can support output coordinates up to 4096 x 4096 pixels. So if the screen falls within this range, there should not be any issue. With that being said, the answer to your second question would be that the device resolution is related to the size of the screen.
Regards,
Aaron