Part Number: ADS1247EVM
Other Parts Discussed in Thread: ADS1247, TIPD120
Hi,
I am currently working with the ADS1247 EVM for an RTD measurement application.
- I have modified the EVM circuit with reference of TIPD120 Design files and the modifications done are attached.
- When I try to read the Analog input, the ADS1247 always returns with zero.
- Differential voltage between AIN1 and AIN2 was measured and noted as 110 mV
- Reference Voltage between REF0P and REF0N was measured and noted as 1.6 V
- The data is polled using the status of DRDY pin.
- The following register settings was used for configuration.
Address Register Value
00h MUX0 0A
01h VBIAS 00
02h MUX1 20
03h SYS0 22
04h OFC0 00
05h OFC1 00
06h OFC2 00
07h FSC0 00
08h FSC1 00
09h FSC2 00
0Ah IDAC0 96
0Bh IDAC1 03
0Ch GPIOCFG 00
0Dh GPIODIR 00
0Eh GPIODAT 00
Thank you in advance for any help you provide.