Part Number: DAC38RF83
Other Parts Discussed in Thread: LMK04616, , LMK04828
Hi
I want to connect the LMK04616 to SYSREF+/-, DACCLK+/- inputs.
The LMK04616 outputs are 8mA HDSD, 4mA HDSD and 16mA HCSL.
Which of the option I need to use and what kind coupling (AC\DC) is needed?
What is the termination I need?
Kind regards,
Shlomi