This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC084S085: OFFLINE REQUEST

Part Number: DAC084S085


Dear Sir:

I'll send you a question, DAC084S085 startup sequence.

When system start DIN and SCLK port voltage of DAC084S085 was midpoint potential voltage.

DAC084S085 was conected to MCU and we found MCU makes midpoint potential voltage.

But I'm confused about this voltage wave, rise rapidly and fall slowly in 500us.

Midpoint potential voltage is VCC/2 for general IC.(VCC is Power supply voltage.)

So please check wave figure and judge this midpoint potential voltage will make risk or not.

I'd send you wave figure, if I get your e-mail immediately.

Sincerely, YUZURU

  • Hello,

    At this point the issue seems a bit unclear. Would it be possible for you to post the waveform or a schematic?

  • DAC084S085_OFFLINE_REQUEST.pdf

    Thank you for your message.

    Sorry, I can't attached Schematic file.

    So I attached PDF of waveform.

    DAC connect MCU directly, no dumping resistor, pulled-up resistor and pulled-down resistor.

    SYNCn = H is fixed during Power ON.

  • Hello,

    I think I understand the situation you are asking about, but I want to be sure.

    The MCU is controlling plots 3 (purple / DAC DIN pin) and 4 (green / DAC SCLK pin). Meanwhile, plot 1 (yellow / DAC VA & VREF) is already stable at 3.3V (although it looks like the plot is 1V / division and something closer to 4.3V).

    For some reason, your MCU has this voltage spike / decay behavior upon powering up the SPI peripheral. The SYNC pin is not pictured.

    Since the VA supply is already stable, there is no violation of the absolute maximum ratings table and therefore I do not see any cause for risk to damage the device. If what you say is true concerning the SYNC pin, then there is also no risk for the device to be accidentally latching input data.