Part Number: AFE4404EVM
Dear TI
1. Why the EVM put an indutor(L1) on the analog input?
Will it not affect the frequency response?
2. The protection diodes(D3~D7) are for ESD or the feedback current of the LED
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE4404EVM
Dear TI
1. Why the EVM put an indutor(L1) on the analog input?
Will it not affect the frequency response?
2. The protection diodes(D3~D7) are for ESD or the feedback current of the LED
Hi Harvey,
L1 is the EVM is the common mode choke which is useful to suppress any high frequency common mode signal. It doesn't do anything to PPG signal.
I would suggest checking the datasheet of L1 for the frequency response.
D3 -D7 are for ESD.
Regards,
Prabin