Part Number: ADS1256
Other Parts Discussed in Thread: ADS1234, ADS1232, , ADS1241, ADS1235, ADS1248, ADS124S08, ADS1261
Hi!
I am redesigning an old board that uses ADS1232/ADS1234, using a faster processor to read scale weight.
One thing that today is a problem is that ADS1232/1234 is very slow and it makes practically impossible for us to acquire more samples to use any existing algorithm to measure moving animals over the platform.
And it's necessary to increase the stability of signals measured on load cells.
Is ADS1256 desireable to be used as a Weight scale AD converter?
if not, or if there is an AD converter faster and suitable to be used as Weight scale converter, what is recommended?
I see another component, ADS1241, and about it?
I Intent to place booth used today and the new one at the same PCB (for compatibility reason).
What is the best recommendation?
Sincerely
Cleber Magalhães