Part Number: DAC38RF80
Tool/software: Code Composer Studio
Hi TI
We want to develop DAC38RF80, but there are too many registers.
Is there any reference code that can help us?
Can it be provided?
Thanks.
Jerry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC38RF80
Tool/software: Code Composer Studio
Hi TI
We want to develop DAC38RF80, but there are too many registers.
Is there any reference code that can help us?
Can it be provided?
Thanks.
Jerry
Hi Jerry,
No, we don't have code available. We do provide a configuration file, which is text based that you have to write code to dump to the device.
Thanks,
Eben.
Hi Jerry,
Configuration attached.
Thanks,
Eben.
DAC38RF8x 0x00 0x5800 0x01 0x3080 0x02 0xFFFF 0x03 0xFFFF 0x04 0x00FE 0x05 0x0003 0x40A 0x7C03 0x40B 0x0002 0x40C 0xA002 0x40D 0xF000 0x41B 0x0000 0x423 0xFFFF 0x424 0x1001 0x431 0x0400 0x432 0x0508 0x433 0x403C 0x434 0x0000 0x435 0x0018 0x43B 0x9002 0x43C 0x8029 0x43D 0x0088 0x43E 0x0909 0x43F 0x0000 0x10A 0x8610 0x10C 0x2732 0x10D 0x0000 0x10E 0x00FF 0x10F 0xFFFF 0x110 0xFFFF 0x111 0xFFFF 0x117 0x0000 0x119 0x0001 0x11C 0x0000 0x11D 0x0000 0x11E 0xC71C 0x11F 0x1C71 0x120 0x2B67 0x121 0xC71C 0x122 0x1C71 0x123 0x2B67 0x124 0x0030 0x125 0x2600 0x127 0x8888 0x128 0x0330 0x129 0x0000 0x12A 0x0000 0x12B 0x0000 0x12C 0x0000 0x12D 0x1FFF 0x12E 0x1FFF 0x12F 0x0000 0x130 0x0000 0x132 0x0400 0x133 0x0400 0x146 0x0044 0x147 0x190A 0x148 0x31C3 0x14A 0x0F02 0x14B 0x1301 0x14C 0x1303 0x14D 0x0300 0x14E 0x0F0F 0x14F 0x1C60 0x150 0x0000 0x151 0x001F 0x152 0x00FF 0x153 0x0100 0x154 0x8E60 0x15C 0x0002 0x15E 0x0000 0x15F 0x3210 0x160 0x5764 0x164 0x0000 0x165 0x0000 0x166 0x0000 0x167 0x0000 0x168 0x0000 0x169 0x0000 0x16A 0x0000 0x16B 0x0000 0x16C 0x0000 0x16D 0x0000 0x16E 0x0000 0x20A 0x8610 0x20C 0x2732 0x20D 0x0000 0x20E 0x00FF 0x20F 0xFFFF 0x210 0xFFFF 0x211 0xFFFF 0x217 0x0000 0x219 0x0001 0x21C 0x0000 0x21D 0x0000 0x21E 0xC71C 0x21F 0x1C71 0x220 0x2B67 0x221 0xC71C 0x222 0x1C71 0x223 0x2B67 0x224 0x0020 0x225 0x2600 0x227 0x8888 0x228 0x0330 0x229 0x0000 0x22A 0x0000 0x22B 0x0000 0x22C 0x0000 0x22D 0x1FFF 0x22E 0x1FFF 0x22F 0x0000 0x230 0x0000 0x232 0x0400 0x233 0x0400 0x246 0x0044 0x247 0x190A 0x248 0x31C3 0x24A 0xF002 0x24B 0x1301 0x24C 0x1303 0x24D 0x0300 0x24E 0x0F0F 0x24F 0x1C60 0x250 0x0000 0x251 0x001F 0x252 0x00FF 0x253 0x0100 0x254 0x8E60 0x25C 0x0003 0x25E 0x0000 0x25F 0x5764 0x260 0x3210 0x264 0x0000 0x265 0x0000 0x266 0x0000 0x267 0x0000 0x268 0x0000 0x269 0x0000 0x26A 0x0000 0x26B 0x0000 0x26C 0x0000 0x26D 0x0000 0x26E 0x0000
Hi Jerry,
The DAC PLL may require some tuning of the VCO code. You may refer to the flow chart for tuning code modification for locking of the PLL/VCO across temperature
For the alarm error, the SERDES to JESD204B RX block has a FIFO in between. The FIFO error indicates that the serdes rate from your FPGA is not matching with the SERDES rate configuration of the DAC. You will need to double check the SERDES.
You may refer to the attached presentation for another similar device and apply the JESD error debug to the DAC38RF8x family.
Hi Jerry,
The DAC PLL may require some tuning of the VCO code. You may refer to the flow chart for tuning code modification for locking of the PLL/VCO across temperature
For the alarm error, the SERDES to JESD204B RX block has a FIFO in between. The FIFO error indicates that the serdes rate from your FPGA is not matching with the SERDES rate configuration of the DAC. You will need to double check the SERDES.
You may refer to the attached presentation for another similar device and apply the JESD error debug to the DAC38RF8x family.
Jan Joe,
This is the VCO varactor adjustment to ensure that we center the VCO such that the VCO stays locked across temperature. You have to tunes this to ensure the loop filter voltage (the bias of the VCO) is within range of the error amplifier of the PLL loop such that the PLL can absorb the up/down of the bias change across temperature. Modification is not invalid. You can always adjust it. Please refer to the flow chart and modify VCO code accordingly to the temperature.
-Kang
Hello,
Just a friendly ping on the debug status. I will close this thread for now since I haven't heard back from you. You can always reply back to inquire further.
below is a picture regarding VCO capacitor array related to the VCO code inquiry you had earlier. This will help you with your understanding.