The datasheet ((SNAS411P –AUGUST 2008–REVISED APRIL 2017) is not very clear about SCLK duty-cycle limits and low/high time requirements; only typical values are given (duty-cycle 40%..60% and SCLK low/high 0.4 times clock time).
- What are the absolute limits for SCLK duty-cycle and low/high times for which the device is still guaranteed to operate?
- It is likely that duty-cycles outside the typical range have an impact on ADC accuracy; can this be specified/estimated?
- Are there other side-effects to consider when the duty-cycle is outside of the typical range?
Any help is appreciated. Thanks.