Other Parts Discussed in Thread: TMS320VC5509A, ADCPRO
Hello, TI community!
I've got some problem when I getting started install USBStyx driver. I have succesfully installed the NI-Visa driver (TMS320VC5509A) and ADCPro (version is 1.1.0). But when I run the ADCPro and clicked the menu for board, it says "DSP not ready... Retrying". I know someone had question like this and it was solved, but I want make sure that am I connected all power supplies and addition ones properly?
I read EVM board's documention and found that the jumper J12 should be disconnected but when I do it the board doesn't works, PC's property menu doesn't show that the connection is fine and the LED D2 doesn't glows. Thats why I connected the J12. I have attached the schematics below. Please don't judge me, I haven't another components and I created scheme for addition supplying to board with those ones that I have.
As you see the values of input voltages there are no perfect. -4,84V for -5VA, and +/- 9,6V to VA+/-. I measured with multimeter. Is that matter be perfect for installing USBStyx driver and make sure that is everything ok? Thank you much!!! Sorry for my bad English!
Best regards,
Osim.