Hi!
I found an error in the PCB and now the PLL DAC is working.
But I had questions on SerDes PLL.
I apply to the DAC data with a frequency of 328 MHz, two IQ pairs. For data transmission, four SerDes lines are used, mode 44210. SerDes lane rate is 6560 MHz. SerDes PLL VCO frequency is 6560 * 0.25 = 1640.
I give the input DACCLK 328 MHz.
Set parameter values:
SERDES_REFCLK_PREDIV = 0,
SERDES_REFCLK_SEL = 0,
RATE = 0,
MPY = 0x28.
In the register DTEST, bits 11: 8 write 0x1. At the ALARM output, I see a frequency of 41 MHz (SerDes PLL VCO frequency is 41 * 80 = 3280), although I expected to see 20.5 MHz (1640/80 = 20.5 MHz).
What am I configuring wrong?
Configuration data read from the DAC:DAC38RF89_config.cfg