Part Number: ADS1298
Hello,
I have been trying to implement the internal test signal of the ADS1298 but I am having issues with it.
1- My register codes for the internal signal generation:
[0x41, 0x00, 0x85] [0x42, 0x00, 0x10] [0x43, 0x00, 0xC8] [0x45, 0x0B, 0x05]
Questions:
1- Why is the test signal only 0.1mV in amplitude? (If I am using the internal reference to 2.4V and gain 6)
1.1 - Why is the signal deviated from 0V?
2- Why is only channel 1 configured for the test signal? (The other channels don't have the correct signal)
3- The spikes I am gessing are the effect of corrupted data from the readings I am acquiring, since some times the DRDY signal goes low during one reading.
4- My internal noise measurements are also deviated from 0V, why is that?
Thank you very much in advance,
Best,
Sofia
----
I have valid readings of the devices ID, I have validated the check points of the circuit, followed the startup advices.
I have nothing connected to the analog input pins of the ADS1298.
I have verified my conversion code from this explanation:
e2e.ti.com/.../2856893