This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSW1400EVM
Hello!
For reading and analysis of high speed analog signals I have wanted to use the ADC1173 Board in combination with TSW1400EVM Evaluation Module. Since this is a parallel ADC it is connected to the TSW1400 board through the CMOS interface.
However, when using the High Speed Data Conversion Software, the software recognizes the TSW1400 Board but not the ADC -> in the "Select ADC" box the adc1173_cmos is not listed.
The software version is v5.00.02 and I have also installed the latest Patch (released in April).
Has anyone encountered the same problem?
Do you have any idea how to solve this?
Thank you for your support!
Sincerely,
T. So
Hi T. So,
For some reason, these files did not get included in this version of HSDC Pro. Please find the missing files, and instructions to add them, attached.
Best Regards,
Dan