Part Number: ADS8668EVM-PDK
need to talk to ads8668 from raspberry pi over spi. Need help regarding what changes has to be made on evm to use external processor.
Any help is appreciated.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8668EVM-PDK
need to talk to ads8668 from raspberry pi over spi. Need help regarding what changes has to be made on evm to use external processor.
Any help is appreciated.
Hello,
Are you using the EVM, or are you using your own PCB?
The EVM User's Guide will be helpful to look at to see how to connect the device. there is a schematic near the end of the document.
The digital pins on the device need to be driven by the processor, this includes
CS, SCLK, SDO, SDI. It is useful to use an oscilloscope to verify the digital communications are in fact what are expected from the firmware
The datasheet timing diagram will be helpful here for comparisons
Be sure to pull pin2 RST high, or else the device will be hardwired to power down mode.
Regards
Cynthia
No, it is not possible to connect the EVM to the communications and connect to the GUI and connect it to the raspberry pi
If you want to use the Raspberry pi, you will need to ONLY use the raspberry pi and create your own software.
It is one or the other, the communication card that came with the EVM and the GUI OR the raspberry pi
Regards
Cynthia