Part Number: ADS1261EVM
Hi Team,
Is it possible to reprogram the TM4C19x processor on the ADS1261EVM to do digital control and filtering for a control loop?
Thanks,
Matt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1261EVM
Hi Team,
Is it possible to reprogram the TM4C19x processor on the ADS1261EVM to do digital control and filtering for a control loop?
Thanks,
Matt
Hi Matt,
With the ICDI on the the EK-TM4C1294XL it is possible to connect to the J7 JTAG connector and re-program the ADS1261EVM.
Please note that while it is possible to make modifications to the ADS1261EVM, it is not something for which we provide applications support. As far as existing code that the customer could reference, I would point them to the ADS1261 Example C Code and the TM4C ARM® Cortex®-M4F MCU (2.1.4.178) software library which provides lots of examples.