Part Number: ADS7142
Dear TI Experts,
My customer is debugging ADS7142, it works well on Manual Mode, however, when it works on Autonomous mode, after set "Start sequence", there will be a short time pulse on the input pin(AINP/AIN0), one-channel, single-ended,even the input signal is 0V. If the DWC is EN, this short time signal wiil trigger the alert then MCU will read this higer ADC value. Is this normal? Could you kindly give some advices about this short time pulse ? Thanks a lot.