This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC1128EVM: Data converters forum

Part Number: DDC1128EVM

ear TI,

I developed a "Daughter" Interface board for DDC1128EVM  for receiving  very low DC signal signal from PCBs photodiode sensors.

I use coaxial cable with SMB connectors to receive the signals of the photodiodes from a distance of around 12 inches. The PCB interface was mounted on the DDC1128EVM, as seen in the attached photo. The results obtained with respect to SNR, etc. and the histograms observed for each sensor show a large dispersion in the repeatability of the sampled signal, i.e., the "bell" shape is far from optimal. (photos attached).

The + 5V Power Supply both digital and analog is very clean with very low ripple. My questions are:

(1) Is it convenient to redesign the PCB interface so that it does not overlap the PCB of the DDC1128EVM in order to avoid contamination (noise) from the digital section of the evaluation board?
(2) According to the experience of other IT clients using the same hardware, would there be any restriction in connecting the photodiodes without previous use of some trans-impedance amplifier?

HISTOGRAMs: Channel 02 and 01, no bell shape; 

 no bell shape;  no bell shape;    This should be a good example of Histogram....

Please, see table below with configuration parameters, and values.

(1) Only the channels 01, 02, 03, 04 were connected to photodiodes (Highlighted in green)

(2) 

Board DDC1128 Daughter Card
7/8/2019 17:23:11
FPGA Configuration
Register Tab
Master CLK 80.0MHz
CONV Low Int 1600 320 uS
CONV High Int 1600 320 uS
CONV selection Free Run Avg: 3.125 kHz
CLK High 7 remember to add 1 for true value
CLK Low 7 remember to add 1 for true value
CLK Freq 5 MHz
CLK Duty 50.000% high
CLK Cfg Running
Format (FPGA) 20 bit
Channel Count 128
/DVALID ignore 255
/DVALID read 1024
Hardware Trigger Disabled
CLK CFG High 3 remember to add 1 for true value
CLK CFG Low 3 remember to add 1 for true value
CLK CFG Freq 10 MHz
CLK Tab
DCLK Tab
DCLK High 0
DCLK Low 0
DCLK Freq 40 MHz
DCLK Duty 50.000% high
DCLK Cfg Running
DCLK Wait 13000
DDC Configuration
Bit 15 0 0
Bit 14 0 0
Bit 13 CLKDIV 0
Bit 12 0 0
Bit 11 0 0
Bit 10 Range[1] 1
Bit 9 Range[0] 1
Bit 8 Format 1
Bit 7 SPEED 0
Bit 6 0 0
Bit 5 0 0
Bit 4 SLEW 0
Bit 3 0 0
Bit 2 0 0
Bit 1 0 0
Bit 0 TEST 0
Codes Codes Codes Codes Codes Codes Codes Codes Codes Codes Codes PPM PPM PPM
Channel Average RMS Noise P2P Noise Min Code Max Code Bits/Chan Vref[V] Range ENOB[RMS] ENOB[P2P]
84A 3929.265625 14.00459432 186 3837 4023 20 4.096 3 16.19217171 12.46084119 -159.6340137 13.40821053 178.0792146
83A 3840.707031 15.38008393 215 3735 3950 20 4.096 3 16.05700853 12.25180715 -244.4213515 14.72512509 205.8442535
82A 3978.636719 16.78694792 208 3862 4070 20 4.096 3 15.93073195 12.29956028 -112.3653814 16.07207796 199.1423475
81A 3820.503906 15.68637896 223 3705 3928 20 4.096 3 16.02855955 12.1991001 -263.7641291 15.01837658 213.5035745
80A 3950.914063 15.70232235 220 3834 4054 20 4.096 3 16.02709396 12.21864029 -138.9074721 15.03364103 210.6313291
79A 3808.998047 14.72515108 192 3716 3908 20 4.096 3 16.11978947 12.4150375 -274.7800129 14.09808247 183.8237054
78A 3942.427734 14.10059605 189 3848 4037 20 4.096 3 16.18231576 12.43775758 -147.032411 13.50012403 180.95146
77A 3821.714844 15.49283902 237 3703 3940 20 4.096 3 16.04647037 12.11125675 -262.6047592 14.83307852 226.9073864
76A 3951.146484 13.87260774 179 3870 4049 20 4.096 3 16.2058329 12.51618422 -138.6849478 13.28184457 171.3773087
75A 3827.400391 15.05179339 209 3720 3929 20 4.096 3 16.08813651 12.29264087 -257.1613306 14.41081476 200.0997627
74A 3945.683594 14.69100638 195 3846 4041 20 4.096 3 16.12313868 12.39266969 -143.915202 14.06539181 186.6959508
73A 3817.753906 13.74566638 190 3718 3908 20 4.096 3 16.21909506 12.43014439 -266.3970207 13.16030899 181.9088751
72A 3959.302734 12.88683286 171 3882 4053 20 4.096 3 16.31217416 12.58214749 -130.8760307 12.33804879 163.7179876
71A 3839.861328 14.13586103 181 3746 3927 20 4.096 3 16.17871214 12.50015411 -245.2310404 13.53388726 173.292139
70A 3971.550781 13.81410339 190 3868 4058 20 4.096 3 16.21192998 12.43014439 -119.1495652 13.22583163 181.9088751
69A 3883.199219 13.80087744 194 3785 3979 20 4.096 3 16.21331191 12.40008716 -203.7386881 13.2131689 185.7385357
68A 4001.746094 13.07871244 182 3915 4097 20 4.096 3 16.29085139 12.49220536 -90.24011612 12.5217572 174.2495541
67A 3888.701172 14.26460869 195 3792 3987 20 4.096 3 16.16563173 12.39266969 -198.471035 13.65715222 186.6959508
66A 4004.8125 14.37554347 200 3901 4101 20 4.096 3 16.15445541 12.35614381 -87.30429238 13.76336285 191.4830265
65A 3900.861328 7.934934907 78 3868 3946 20 4.096 3 17.01178161 13.71459778 -186.8287174 7.597026754 74.67838032
64A 3994.3125 15.48588067 202 3896 4098 20 4.096 3 16.04711848 12.34178852 -97.35715127 14.82641649 193.3978567
63A 3878.095703 15.16551331 196 3778 3974 20 4.096 3 16.07727757 12.38529016 -208.6248712 14.51969194 187.6533659
62A 4025.960938 15.1501095 183 3927 4110 20 4.096 3 16.07874368 12.48430016 -67.05645829 14.50494409 175.2069692
61A 3861.935547 5.746070846 41 3842 3883 20 4.096 3 17.47742422 14.642448 -224.0968494 5.50137518 39.25402043
60A 3978.734375 6.43960448 46 3958 4004 20 4.096 3 17.31302792 14.47643804 -112.2718839 6.165374775 44.04109609
59A 3871.775391 6.75653184 58 3848 3906 20 4.096 3 17.24371711 14.142019 -214.6760341 6.468805826 55.53007768
58A 3968.318359 15.30185264 208 3851 4059 20 4.096 3 16.06436557 12.29956028 -122.2443349 14.65022527 199.1423475
57A 3854.367188 15.55917188 217 3735 3952 20 4.096 3 16.04030663 12.23844877 -231.3429112 14.8965866 207.7590837
56A 3960.669922 15.65666896 210 3852 4062 20 4.096 3 16.0312946 12.28575448 -129.5670647 14.98993178 201.0571778
55A 3825.076172 12.86878106 161 3743 3904 20 4.096 3 16.3141965 12.66908312 -259.3865728 12.32076572 154.1438363
54A 3945.751953 8.655685682 86 3905 3991 20 4.096 3 16.88635189 13.57373525 -143.8497537 8.287084452 82.33770138
53A 3858.851563 13.83670946 184 3757 3941 20 4.096 3 16.20957101 12.47643804 -227.0495027 13.24747502 176.1643843
52A 3953.554688 14.29573723 200 3845 4045 20 4.096 3 16.16248688 12.35614381 -136.3792977 13.68695515 191.4830265
51A 3865.810547 14.73997428 205 3763 3968 20 4.096 3 16.1183379 12.3205199 -220.3868657 14.11227443 196.2701021
50A 3953.570313 13.6142065 184 3865 4049 20 4.096 3 16.23295901 12.47643804 -136.3643381 13.03444732 176.1643843
49A 3863.886719 14.04286335 192 3764 3956 20 4.096 3 16.18823477 12.4150375 -222.2287679 13.44484987 183.8237054
48A 3968.554688 13.2190432 177 3879 4056 20 4.096 3 16.27545415 12.53239445 -122.0180707 12.65611199 169.4624784
47A 3855.296875 14.48509977 195 3754 3949 20 4.096 3 16.14350228 12.39266969 -230.4528143 13.86825371 186.6959508
46A 3979.587891 13.27621558 177 3891 4068 20 4.096 3 16.26922794 12.53239445 -111.4547151 12.7108497 169.4624784
45A 3880.648438 13.31988636 178 3793 3971 20 4.096 3 16.26449013 12.52426657 -206.1808447 12.75266076 170.4198936
44A 3986.685547 14.24892903 197 3891 4088 20 4.096 3 16.16721842 12.37794818 -104.6593116 13.64214028 188.6107811
43A 3873.767578 14.34121994 183 3780 3963 20 4.096 3 16.15790415 12.48430016 -212.7686836 13.73050099 175.2069692
42A 3989.761719 14.70284635 190 3900 4090 20 4.096 3 16.12197643 12.43014439 -101.7141381 14.07672758 181.9088751
41A 3882.810547 13.8393844 184 3787 3971 20 4.096 3 16.20929213 12.47643804 -204.1108085 13.25003605 176.1643843
40A 3985.701172 11.37287749 140 3914 4054 20 4.096 3 16.49247458 12.87071698 -105.6017671 10.88856501 134.0381185
39A 3898.427734 11.10209424 148 3831 3979 20 4.096 3 16.52724006 12.79054663 -189.1586768 10.62931302 141.6974396
38A 4000.302734 13.00270977 180 3909 4089 20 4.096 3 16.29925959 12.5081469 -91.62201023 12.44899109 172.3347238
37A 3900.412109 10.41014801 140 3834 3974 20 4.096 3 16.62008132 12.87071698 -187.2588062 9.96683323 134.0381185
36A 4031.351563 13.06464686 170 3937 4107 20 4.096 3 16.29240378 12.59060906 -61.89539234 12.5082906 162.7605725
35A 3942.095703 12.72595086 158 3866 4024 20 4.096 3 16.33029845 12.69621925 -147.3503028 12.18401793 151.2715909
34A 4035.654297 12.43324445 154 3963 4117 20 4.096 3 16.36386909 12.73321346 -57.77588934 11.90377638 147.4419304
33A 3960.341797 11.62190698 158 3889 4047 20 4.096 3 16.46122509 12.69621925 -129.8812165 11.12698961 151.2715909
32A 4017.998047 10.30785862 142 3948 4090 20 4.096 3 16.63432725 12.85025288 -74.68025027 9.868899824 135.9529488
31A 3901.929688 14.86984343 200 3793 3993 20 4.096 3 16.10568245 12.35614381 -185.8058539 14.23661312 191.4830265
30A 3998.548828 6.265726978 52 3968 4020 20 4.096 3 17.35251809 14.29956028 -93.30122662 5.998901824 49.78558688
29A 3876.398438 13.71492107 167 3793 3960 20 4.096 3 16.22232559 12.61629571 -210.249859 13.13087297 159.8883271
28A 3975.888672 15.466108 213 3868 4081 20 4.096 3 16.04896171 12.26529038 -114.9964031 14.80748584 203.9294232
27A 3850.357422 7.075429508 63 3819 3882 20 4.096 3 17.17718227 14.02272008 -235.1819214 6.774123279 60.31715334
26A 3973.896484 7.303348129 73 3935 4008 20 4.096 3 17.131442 13.81017544 -116.9037536 6.992336015 69.89130466
25A 3845.386719 6.593887689 48 3826 3874 20 4.096 3 17.27887069 14.4150375 -239.9409478 6.313087855 45.95592635
24A 3984.970703 15.32005939 202 3877 4079 20 4.096 3 16.06265001 12.34178852 -106.301129 14.66765669 193.3978567
23A 3834.082031 14.65372144 208 3719 3927 20 4.096 3 16.12680481 12.29956028 -250.7642267 14.02969465 199.1423475
22A 3957.671875 15.85326237 213 3845 4058 20 4.096 3 16.01329215 12.26529038 -132.4374401 15.17815329 203.9294232
21A 3842.568359 15.00062547 209 3739 3948 20 4.096 3 16.09304925 12.29264087 -242.6392877 14.36182582 200.0997627
20A 3967.310547 14.82618191 210 3862 4072 20 4.096 3 16.10992479 12.28575448 -123.2092298 14.19481091 201.0571778
19A 3858.759766 14.99996427 207 3754 3961 20 4.096 3 16.09311284 12.30651304 -227.1373904 14.36119278 198.1849324
18A 3972.740234 15.37477459 202 3872 4074 20 4.096 3 16.05750665 12.34178852 -118.0107648 14.72004185 193.3978567
17A 3850.769531 7.482636762 73 3810 3883 20 4.096 3 17.09645326 13.81017544 -234.7873617 7.163989665 69.89130466
16A 3993.396484 13.35969581 173 3908 4081 20 4.096 3 16.26018475 12.56537177 -98.23415849 12.79077493 165.6328179
15A 3869.914063 12.95381058 169 3789 3958 20 4.096 3 16.30469535 12.59912056 -216.4580978 12.40217427 161.8031574
14A 3983.308594 15.6409445 197 3889 4086 20 4.096 3 16.03274427 12.37794818 -107.8924576 14.97487695 188.6107811
13A 3867.675781 15.25500556 216 3763 3979 20 4.096 3 16.0687892 12.2451125 -218.6010621 14.60537317 206.8016686
12A 3998.640625 14.60146845 189 3903 4092 20 4.096 3 16.13195844 12.43775758 -93.2133389 13.97966685 180.95146
11A 3881.753906 10.53741401 124 3822 3946 20 4.096 3 16.60255105 13.04580369 -205.1224522 10.08867963 118.7194764
10A 4017.705078 13.56094942 179 3929 4108 20 4.096 3 16.23861372 12.51618422 -74.96074299 12.98345818 171.3773087
09A 3870.060547 13.46241317 177 3778 3955 20 4.096 3 16.24913487 12.53239445 -216.3178514 12.88911809 169.4624784
08A 4011.375 12.64926505 162 3932 4094 20 4.096 3 16.33901834 12.66015 -81.02125557 12.11059777 155.1012514
07A 3902.617188 14.77321853 212 3787 3999 20 4.096 3 16.11508774 12.27207955 -185.147631 14.14410298 202.9720081
06A 4035.503906 8.742853352 98 3988 4086 20 4.096 3 16.8718958 13.38529016 -57.9198756 8.370540099 93.82668297
05A 3916.371094 12.06326845 154 3845 3999 20 4.096 3 16.40745106 12.73321346 -171.979433 11.54955576 147.4419304
04A 175909.6953 231.7818987 1351 175245 176596 20 4.096 3 12.14337591 9.600188041 164497.0318 221.9114972 1293.467844
03A 170239.8184 233.8300001 1513 169499 171012 20 4.096 3 12.13068377 9.436803728 159068.6058 223.8723805 1448.569095
02A 170397.3086 223.4149169 1547 169642 171189 20 4.096 3 12.1964183 9.404742519 159219.3894 213.9008222 1481.12121
01A 170921.2383 232.8233594 1318 170325 171643 20 4.096 3 12.136908 9.635865345 159721.0076 222.9086074 1261.873144
84B 3975.595703 14.13545731 223 3867 4090 20 4.096 3 16.17875335 12.1991001 -115.2768958 13.53350073 213.5035745
83B 3843.298828 15.40160803 230 3736 3966 20 4.096 3 16.05499092 12.15450995 -241.9399259 14.74573259 220.2054804
82B 3944.238281 16.52430322 241 3837 4078 20 4.096 3 15.95348247 12.08711066 -145.298966 15.82061796 230.7370469
81B 3846.285156 16.48237501 254 3733 3987 20 4.096 3 15.95714776 12.01131531 -239.0807702 15.78047525 243.1834436
80B 3961.916016 16.07801954 250 3844 4094 20 4.096 3 15.9929822 12.03421572 -128.3740356 15.3933392 239.3537831
79B 3876.042969 14.96500179 232 3766 3998 20 4.096 3 16.09647945 12.142019 -210.5901902 14.32771917 222.1203107
78B 3977.117188 14.62172565 220 3869 4089 20 4.096 3 16.12995832 12.21864029 -113.8202037 13.99906139 210.6313291
77B 3858.925781 16.00446591 246 3749 3995 20 4.096 3 15.99959737 12.05748549 -226.9784445 15.32291785 235.5241226
76B 3978.894531 13.45233953 197 3883 4080 20 4.096 3 16.25021481 12.37794818 -112.1185479 12.87947343 188.6107811
75B 3859.109375 15.5395083 245 3746 3991 20 4.096 3 16.04213105 12.06336206 -226.8026691 14.8777604 234.5667074
74B 3952.46875 14.31137414 214 3857 4071 20 4.096 3 16.1609097 12.25853301 -137.4189907 13.70192616 204.8868383
73B 3850.806641 14.22955341 226 3741 3967 20 4.096 3 16.16918152 12.17982104 -234.7518326 13.62358976 216.3758199
72B 3948.822266 12.82185833 192 3850 4042 20 4.096 3 16.31946653 12.4150375 -140.91019 12.27584119 183.8237054
71B 3852.447266 14.11106726 210 3758 3968 20 4.096 3 16.1812448 12.28575448 -233.1810734 13.51014932 201.0571778
70B 3948.138672 14.04715512 223 3851 4074 20 4.096 3 16.18779392 12.1991001 -141.564673 13.44895888 213.5035745
69B 3852.402344 14.1996862 226 3747 3973 20 4.096 3 16.17221286 12.17982104 -233.2240823 13.59499444 216.3758199
68B 3988.150391 13.07560795 196 3891 4087 20 4.096 3 16.29119388 12.38529016 -103.256848 12.51878492 187.6533659
67B 3870.972656 14.65739049 235 3764 3999 20 4.096 3 16.12644363 12.12348305 -215.4445841 14.03320746 224.9925561
66B 3984.355469 14.66815912 225 3887 4112 20 4.096 3 16.12538408 12.18621881 -106.8901637 14.0435175 215.4184048
65B 3873.236328 8.26778437 87 3824 3911 20 4.096 3 16.95249924 13.5570565 -213.2773104 7.915701867 83.29511651
64B 3965.552734 15.51942937 246 3846 4092 20 4.096 3 16.04399639 12.05748549 -124.8921861 14.85853652 235.5241226
63B 3843.357422 15.90042205 234 3734 3968 20 4.096 3 16.00900684 12.12963528 -241.8838274 15.22330468 224.035141
62B 3900.140625 15.3021569 216 3803 4019 20 4.096 3 16.06433688 12.2451125 -187.5187294 14.65051658 206.8016686
61B 3855.267578 5.579388302 36 3836 3872 20 4.096 3 17.51989304 14.830075 -230.4808635 5.341790789 34.46694476
60B 3943.087891 6.356444337 48 3917 3965 20 4.096 3 17.33178002 14.4150375 -146.4003674 6.085755996 45.95592635
59B 3860.574219 7.050761773 80 3821 3901 20 4.096 3 17.18222086 13.67807191 -225.4002055 6.750506016 76.59321059
58B 3944.007813 14.99739357 249 3830 4079 20 4.096 3 16.09336011 12.03999807 -145.5196203 14.35873155 238.3963679
57B 3844.162109 15.58141076 239 3736 3975 20 4.096 3 16.03824604 12.09913319 -241.1134074 14.91787844 228.8222166
56B 3961.625 15.82262522 250 3832 4082 20 4.096 3 16.01608292 12.03421572 -128.6526584 15.14882082 239.3537831
55B 3854.53125 13.4570715 203 3752 3955 20 4.096 3 16.24970742 12.33466408 -231.1858352 12.88400389 194.3552719
54B 3965.484375 9.291069616 120 3903 4023 20 4.096 3 16.78415531 13.0931094 -124.9576344 8.895410646 114.8898159
53B 3847.462891 14.20464925 215 3742 3957 20 4.096 3 16.1717087 12.25180715 -237.9531895 13.59974614 205.8442535
52B 3967.572266 15.65879634 249 3850 4099 20 4.096 3 16.03109859 12.03999807 -122.9586563 14.99196857 238.3963679
51B 3859.117188 14.92997776 232 3745 3977 20 4.096 3 16.09985989 12.142019 -226.7951893 14.29418663 222.1203107
50B 3983.429688 13.99228783 195 3881 4076 20 4.096 3 16.19344003 12.39266969 -107.7765206 13.3964281 186.6959508
49B 3866.476563 13.81262152 205 3768 3973 20 4.096 3 16.21208475 12.3205199 -219.7492123 13.22441286 196.2701021
48B 3986.804688 13.58756819 214 3880 4094 20 4.096 3 16.23578463 12.25853301 -104.5452446 13.0089434 204.8868383
47B 3884.572266 15.05480393 231 3766 3997 20 4.096 3 16.08784799 12.14825096 -202.4241123 14.4136971 221.1628956
46B 3990.759766 13.67946762 198 3893 4091 20 4.096 3 16.22605982 12.37064338 -100.7585929 13.0969293 189.5681962
45B 3868.423828 13.31096157 208 3761 3969 20 4.096 3 16.26545711 12.29956028 -217.8848707 12.74411603 199.1423475
44B 3960.382813 15.05478075 222 3844 4066 20 4.096 3 16.08785021 12.20558413 -129.8419475 14.4136749 212.5461594
43B 3865.753906 14.61330944 222 3758 3980 20 4.096 3 16.13078897 12.20558413 -220.4410943 13.99100359 212.5461594
42B 3991.546875 14.68170597 236 3869 4105 20 4.096 3 16.12405229 12.11735695 -100.0050025 14.05648747 225.9499712
41B 3851.214844 13.92027854 212 3747 3959 20 4.096 3 16.20088383 12.27207955 -234.3610128 13.32748532 202.9720081
40B 4015.146484 12.13820268 169 3929 4098 20 4.096 3 16.39851709 12.59912056 -77.41037936 11.62129892 161.8031574
39B 3857.505859 10.91980555 151 3781 3932 20 4.096 3 16.55112474 12.76159526 -228.3378992 10.45478707 144.569685
38B 3989.412109 13.46189972 215 3888 4103 20 4.096 3 16.24918989 12.25180715 -102.0488594 12.8886265 205.8442535
37B 3861.302734 10.61194751 141 3780 3921 20 4.096 3 16.59238246 12.86044865 -224.7027136 10.16003913 134.9955337
36B 3995.730469 13.49398048 208 3898 4106 20 4.096 3 16.24575593 12.29956028 -95.99956653 12.91934111 199.1423475
35B 3887.876953 12.86963238 171 3796 3967 20 4.096 3 16.31410106 12.58214749 -199.2601545 12.32158079 163.7179876
34B 4024.664063 13.07253045 179 3937 4116 20 4.096 3 16.29153347 12.51618422 -68.29810604 12.51583847 171.3773087
33B 3901.091797 11.53566866 163 3816 3979 20 4.096 3 16.47197027 12.65127185 -186.6080631 11.04442374 156.0586666
32B 3957.587891 10.11632006 141 3888 4029 20 4.096 3 16.66138732 12.86044865 -132.517848 9.685517906 134.9955337
31B 3827.722656 15.13652822 223 3741 3964 20 4.096 3 16.08003756 12.1991001 -256.8527886 14.49194117 213.5035745
30B 3969.601563 7.140432677 57 3939 3996 20 4.096 3 17.1639885 14.16710999 -121.0157768 6.836358296 54.57266254
29B 3846.412109 13.85598676 193 3752 3945 20 4.096 3 16.20756245 12.40754296 -238.9592233 13.26593139 184.7811205
28B 3970.923828 15.46013202 242 3858 4100 20 4.096 3 16.04951927 12.08113676 -119.7498196 14.80176435 231.694462
27B 3841.273438 7.170049298 67 3808 3875 20 4.096 3 17.15801696 13.93391081 -243.8790655 6.864713697 64.14681387
26B 3963.28125 7.242115864 84 3924 4008 20 4.096 3 17.14358874 13.60768258 -127.0669396 6.933711318 80.42287112
25B 3851.644531 6.451335964 55 3820 3875 20 4.096 3 17.31040205 14.21864029 -233.9496234 6.176606675 52.65783228
24B 3982.691406 15.69031612 235 3867 4102 20 4.096 3 16.02819749 12.12348305 -108.4833623 15.02214608 224.9925561
23B 3858.046875 15.22647231 235 3746 3981 20 4.096 3 16.07149017 12.12348305 -227.8199227 14.578055 224.9925561
22B 3983.230469 16.87342612 264 3851 4115 20 4.096 3 15.92331896 11.95560588 -107.9672557 16.15487351 252.7575949
21B 3854.3125 15.34919074 240 3742 3982 20 4.096 3 16.05990931 12.0931094 -231.3952698 14.69554748 229.7796318
20B 3982.695313 15.05889926 248 3860 4108 20 4.096 3 16.08745559 12.04580369 -108.4796224 14.41761802 237.4389528
19B 3861.712891 15.65027923 246 3747 3993 20 4.096 3 16.03188351 12.05748549 -224.3100238 14.98381416 235.5241226
18B 3988.166016 15.72473722 241 3865 4106 20 4.096 3 16.025036 12.08711066 -103.2418884 15.05510137 230.7370469
17B 3873.035156 7.580733081 85 3828 3913 20 4.096 3 17.07766263 13.59060906 -213.4699154 7.257908565 81.38028625
16B 3993.855469 14.19749818 191 3895 4086 20 4.096 3 16.17243518 12.42257117 -97.7947199 13.5928996 182.8662903
15B 3865.525391 13.12705861 176 3765 3941 20 4.096 3 16.28552822 12.54056838 -220.6598786 12.56804456 168.5050633
14B 4001.257813 15.94913599 248 3879 4127 20 4.096 3 16.00459363 12.04580369 -90.70760398 15.26994415 237.4389528
13B 3881.005859 15.86336818 249 3748 3997 20 4.096 3 16.01237278 12.03999807 -205.8386436 15.18782875 238.3963679
12B 3980.054688 14.71091676 242 3869 4111 20 4.096 3 16.12118475 12.08113676 -111.0077967 14.08445431 231.694462
11B 3858.078125 10.86519628 160 3780 3940 20 4.096 3 16.55835767 12.67807191 -227.7900034 10.40250334 153.1864212
10B 3995.25 14.09149788 212 3890 4102 20 4.096 3 16.18324693 12.27207955 -96.45957458 13.49141331 202.9720081
09B 3874.089844 13.41173891 200 3777 3977 20 4.096 3 16.2545756 12.35614381 -212.4601416 12.84060178 191.4830265
08B 4022.453125 13.28201285 197 3920 4117 20 4.096 3 16.26859811 12.37794818 -70.41489106 12.71640009 188.6107811
07B 3879.589844 14.88890285 240 3766 4006 20 4.096 3 16.10383446 12.0931094 -207.1943584 14.25486089 229.7796318
06B 4004.898438 9.40980194 124 3945 4069 20 4.096 3 16.76583564 13.04580369 -87.22201452 9.00908677 118.7194764
05B 3886.310547 11.71500966 167 3796 3963 20 4.096 3 16.44971376 12.61629571 -200.7598555 11.21612752 159.8883271
04B 172885.8223 233.4730764 1297 172185 173482 20 4.096 3 12.13288762 9.659037236 161601.93 223.5306563 1241.767427
03B 168510.418 220.4547083 1309 167810 169119 20 4.096 3 12.21566152 9.645750618 157412.8517 211.0666738 1253.256408
02B 168577.1836 224.4432032 1393 167848 169241 20 4.096 3 12.1897934 9.556020457 157476.7742 214.8853191 1333.679279
01B 170053.3105 223.4928761 1281 169353 170634 20 4.096 3 12.19591496 9.67694524 158890.0404 213.9754616 1226.448785

Thanks in advance.

Regards,

            Mario Marcoccia

IDSI - http://www.imds.com
1291-B NW 65th Place
Ft. Lauderdale, FL 33309
USA