Hello,
My customer would like to use single ended DACCLK.
However, default of SEL_EXTCLK_DIFFSE bit of CLK_PLL_CFG register is 0 = differential.
The Figure 141 in the datasheet says “Provide a clock to the differential or single ended clock input” then “Toggle RESETB pin low then high (recommended pulse duration >10us)”.
Even default is differential DACCLK, providing single ended DACCLK before toggling RESETB is really OK?
DAC38RF8X start up propery?
Best regards,
K.Hirano