Part Number: ADS1115-Q1
Hi,
The problem we are facing now is: the sampling data error is relatively large, as shown in the following diagram:
Vb sampled a negative pressure value. Initially, FSR was 101: FSR = ±0.256 V for measurement and sampling, and the data error was relatively small (ADC input voltage < 0.256V).
Now the ADC input voltage is about 0.7v, and FSR is configured as: 011: FSR = ± 1.024v for sampling, what may be the reason?
Thanks!