Other Parts Discussed in Thread: DAC101C081
Question 1: Does the A group address correspond to the setting of the DAC101C085? Does the group B address correspond to the setting of the DAC101C081?
Question 2: ADR0 of DAC101C081 has three configurations, as shown in box C. Among them, floating and GND are configured in the same way, and the corresponding addresses are the same. As shown in box D, the ADR0 configuration of DAC101C081 is only two effective? What is the significance of writing 3 here?
Question 3: The address configuration pin of DAC101C081 is only one ADR0, so only the three configurations shown in C are selected (the three configurations are all "-"). Why are there different addresses? As shown in the box D.
Question 4: This table lists the address bits of A6-A0, plus a 1-bit read/write flag to form the completion address. As an example, is it correct?
Binary Hexadecimal
Address example: 1000110
Write address: 10001100 0x8C
Read address: 10001101 0x8D