Part Number: ADS1262EVM-PDK
Hello,
I am in the process of evaluating the ADS1262EVM-PDK. I changed the supplied LabView code to allow streaming the data for longer data collections. The LabView functions make calls to some lower level code which TI does not appear to provide the source for. I started running a controlled temperature stability test, holding the temperature constant while monitoring the evaluation board. What I am seeing is steps in values that are reported.
If I had to guess, it appears that the underlying code that I don't seem to have the source for, may monitor the IC's temperature and run some sort of calibration if the temperature changes by some amount.
Is it possible that this question could be passed onto the group that developed the lower level code and see if they could confirm what I am seeing. It's not a problem if this is what is happening. I just want to understand why it is behaving this way.
Thanks.