Hi,
my customer use amc1306 to do phase current sensing in motor drive project as below:
and the schematics is same as datasheet.
but they found when current is zero, switch on the high-side and low-side IGBT, the sampling result will change as below:
the "1, 3,5,7,9" is when low-side IGBT is on while "2,4,6,8" is when low-side IGBT is off.
Could you please tell me, what's the problem? thanks!
Yuan