Part Number: ADS8866
Hello,
I have a problem with the nonlinearity of the ADS8866. In the picture bewlow you can see a Bending of the data (at around 17000 bits). I drive the ADC with a precise function generator, generating a triangle signal at around 1 kHz. The ADC itself is running at around 80kHz via SPI connection.
The schematics of the ADC are shown here:
VCC is 3.3V, supplied by a laboratory power supply. I tested the stability of AVDD and DVDD, but it seems to be stable.
Can you help me with this issue somehow?